Webinar Details:
Avnet engineers are joined by test experts from Rohde & Schwarz to demonstrate OTA modulation analysis techniques using a benchtop compact antenna test range (CATR). The device-under-test combines the AMD Zynq™ RFSoC DFE, featuring multi-channel direct-RF data converters, MATLAB-based 5G NR signal generation, and beamforming through the Fujikura FutureAccess™ mmWave phased array antenna module.
In this Webinar you will learn:
Speakers:
Matt Brown
Technical Director, Avnet
Matthew Brown is a member of Avnet Embedded working in the Advanced Applications Group to speed prototype and deployment of 5G/Satcom systems, pairing AMD RFSoC radio-on-chip with MATLAB and Simulink from Mathworks
Fabrício Dourado
Senior Application Engineer, Rohde & Schwarz
Fabrício Dourado is a senior application engineer at the Rohde & Schwarz (R&S) Headquarters in Munich, Germany. He joined the company in 1996 and worked in various test and measurement product marketing and technical support roles for Europe, the Americas and Asia.
Fabrício primarily focused on Asia from 2001 to 2019, regularly meeting customers and system integrators, sharing our experiences, and involving them in the R&S process to further develop products and automated test systems. He started specializing in mobile radio and production line remote control testing. Later, component tests up to 500GHz, multi-port network analysis, and radio fr ont-ends (RFFE) test. Fabrício joined the R&S Test & Measurement Application Development in April 2020, focusing on 5G-NR, automotive radar, and over-the-air (OTA) testing. Before joining R&S, he worked at the Institute of Materials Research at the German Aerospace Center (DLR) in Cologne, automating the Hall facility for semiconductor thermoelectric characterization.
Fabrício holds a degree in electronics engineering from the Instituto Tecnológico de Aeronáutica in São José dos Campos, Brazil.